Part Number: MSPM0G1507
Tool/software:
Hi,
- I have imported Boot_application and Bin_sample image CCS 20.2.0 Development tool.
- Compile both firmware
- Run debug on Boot Application
- Load via Memory view the bin file of Bim_Sample
The I start deduggin with F10 and F11 and i see the source code till the program reach the istruction to jump to Application Code
Naturally after that i do not see any more the source code 'C'
Is there a way to debug also the source code of application of only the that one.
At end it should be correct do not see the code of Boot but debug the code of application.
Best regard
Massimo