Part Number: MSPM0G1519
Other Parts Discussed in Thread: SHA-256
Tool/software:
Champs,
I have been testing password-protected SWD connection to the Launchpad and found that it seems to be working correctly while working with projects in CCS: I can flash the project with SWD password configured and it works fine, I can also change password and attempt debugging without flashing and it refuse connection. To me it seems to be working as expected.
What I would also want to do is to configure password in the target config file and test connection - this part does not seem to be functional. in the target config I see only 128-bit password field which makes me think this only applies to the older devices that stored 128-bit password directly (vs 256-bit hash). is this the case or I am doing something wrong?
if it is indeed not yet supported - when do we expect this support to be implemented?
thank you
Michael