This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCU-PLUS-SDK-AM243X: Unexpected DCP responses

Part Number: MCU-PLUS-SDK-AM243X

Tool/software:

Hi Laxman

I'm now using ind_comms_sdk_am243x_11_00_00_08. When sending a DCP request with device MAC address as destination address to port 1 or 2 of DUT the expected DCP response is sent by DUT. Let's say, device MAC address of DUT is xx:xx:xx:00:00:00. If a DCP request with MAC address of port 1 (xx:xx:xx:00:00:01) as destination address is sent to port 1 of DUT, there is also a DCP response sent by DUT on port 1. The same with port 2, if a DCP request with MAC address of port 2 (xx:xx:xx:00:00:02) as destination address is sent to port 2 of DUT, there is also a DCP response sent by DUT on port 2. I think, that is not correct. Only DCP request with device MAC address should be forwarded to profinet stack.

Regards, Joachim