Part Number: MSPM0G3507
Other Parts Discussed in Thread: TMDSEMU110-U
Tool/software:
Hi champs,
I am asking this.
Would you please help confirm, if the user wants to use TMDSEMU110-U to program MSPM0 series like G3507, what pins from TMDSEMU110-U should they use?
1. Are SWDIO (Pin1) and SWCLK (Pin11) from the two signals below?

2. We are confused, what is used for NRST?
Is it Pin 2 (nTRST) or Pin 15 (nRESET)?
3. What pins from XDS110 should be used as 3.3V/GND for G3507's VSS and GND?
It's not clear which pin is 3.3V from XDS110?
Would you please confirm?