Part Number: ARM-CGT
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi team,
I'm reporting this issue when adding ADCBuf driver into CC2745-Q1 demo.
The SDK version is SDK 9.11.1.19.
Compiler version is ti-cgt-armllvm_4.0.
I add ADCBuf in the sysconfig and then add a app_driver.c into the project:
#include <string.h>
#include <stdarg.h>
#include "ti_drivers_config.h" // sysconfig
#include <ti/drivers/ADCBuf.h> // driver
#include "ti/ble/app_util/framework/bleapputil_api.h"
#include <app_main.h>
// Define name for ADCBuf channel index
#define PIEZOMETER_OUT 0
// Create buffer for samples
#define ADCBUFFERSIZE 10
uint16_t buffer[ADCBUFFERSIZE];
uint32_t microvoltBuffer[ADCBUFFERSIZE];
bStatus_t Driver_start(void)
{
bStatus_t status = SUCCESS;
// One time init of ADCBuf driver
ADCBuf_init();
// Initialize optional ADCBuf parameters
ADCBuf_Handle adcBufHandle;
ADCBuf_Params params;
ADCBuf_Params_init(¶ms);
params.returnMode = ADCBuf_RETURN_MODE_BLOCKING;
params.recurrenceMode = ADCBuf_RECURRENCE_MODE_ONE_SHOT;
// Open ADCBuf driver
adcBufHandle = ADCBuf_open(CONFIG_ADCBUF_0, ¶ms);
if (adcBufHandle == NULL)
{
//ADCBuf_open() failed.
while (1) {}
}
return status;
}
The compile log is
[264]Building target: "basic_ble_LP_EM_CC2745R10_Q1_freertos_ticlang.out" [265]Invoking: Arm Linker [266]"C:/ti/ti-cgt-armllvm_4.0.4.LTS/bin/tiarmclang.exe" @"C:/ti/simplelink_lowpower_f3_sdk_9_11_01_19/source/ti/ble/stack_util/config/build_components.opt" @"C:/ti/simplelink_lowpower_f3_sdk_9_11_01_19/source/ti/ble/stack_util/config/factory_config.opt" -mcpu=cortex-m33 -mfloat-abi=hard -mfpu=fpv5-sp-d16 -mlittle-endian -mthumb -Oz -DICALL_NO_APP_EVENTS -DCC23X0 -DUSE_HSM -DNVOCMP_NWSAMEITEM=1 -DNVOCMP_NVPAGES=6 -DFREERTOS -DNVOCMP_POSIX_MUTEX -gdwarf-3 -Wunused-function -ffunction-sections -Wl,-m"basic_ble_LP_EM_CC2745R10_Q1_freertos_ticlang.map" -Wl,-i"C:/ti/simplelink_lowpower_f3_sdk_9_11_01_19/source" -Wl,-i"C:/Users/A0503807/Valeo-CC2745/basic_ble_LP_EM_CC2745R10_Q1_freertos_ticlang/Release/syscfg" -Wl,-i"C:/ti/ti-cgt-armllvm_4.0.4.LTS/lib" -Wl,--reread_libs -Wl,--diag_wrap=off -Wl,--display_error_number -Wl,--warn_sections -Wl,--xml_link_info="basic_ble_LP_EM_CC2745R10_Q1_freertos_ticlang_linkInfo.xml" -Wl,--rom_model -o "basic_ble_LP_EM_CC2745R10_Q1_freertos_ticlang.out" "./syscfg/ti_ble_config.o" "./syscfg/ti_devices_config.o" "./syscfg/ti_radio_config.o" "./syscfg/ti_drivers_config.o" "./syscfg/ti_freertos_config.o" "./syscfg/ti_freertos_portable_config.o" "./main_freertos.o" "./HealthToolkit/debugInfo.o" "./app/Profiles/app_dev_info.o" "./app/Profiles/app_simple_gatt.o" "./app/app_broadcaster.o" "./app/app_central.o" "./app/app_connection.o" "./app/app_data.o" "./app/app_driver.o" "./app/app_l2cap_coc.o" "./app/app_main.o" "./app/app_menu.o" "./app/app_observer.o" "./app/app_pairing.o" "./app/app_peripheral.o" "./common/BLEAppUtil/bleapputil_init.o" "./common/BLEAppUtil/bleapputil_process.o" "./common/BLEAppUtil/bleapputil_stack_callbacks.o" "./common/BLEAppUtil/bleapputil_task.o" "./common/BLEAppUtil/bleapputil_timers.o" "./common/Drivers/NV/crc.o" "./common/Drivers/NV/nvocmp.o" "./common/MenuModule/menu_module.o" "./common/Profiles/simple_gatt/simple_gatt_profile.o" "./common/Services/dev_info/dev_info_service.o" "./common/Startup/osal_icall_ble.o" "./common/Startup/rom_init.o" "./common/config/ble_user_config.o" "./common/config/hci_supported_cmd.o" "./common/iCall/icall_POSIX.o" "./common/iCall/icall_cc23x0.o" "./common/iCall/icall_user_config.o" "./common/lib_opt/ctrl_opt_adaptivity.o" "./common/lib_opt/ctrl_opt_adv_conn.o" "./common/lib_opt/ctrl_opt_adv_nconn.o" "./common/lib_opt/ctrl_opt_ae.o" "./common/lib_opt/ctrl_opt_ble_health.o" "./common/lib_opt/ctrl_opt_cm.o" "./common/lib_opt/ctrl_opt_connectable.o" "./common/lib_opt/ctrl_opt_connection_handover.o" "./common/lib_opt/ctrl_opt_cs.o" "./common/lib_opt/ctrl_opt_cs_test.o" "./common/lib_opt/ctrl_opt_health_check.o" "./common/lib_opt/ctrl_opt_initiator.o" "./common/lib_opt/ctrl_opt_legacy_cmd.o" "./common/lib_opt/ctrl_opt_padv.o" "./common/lib_opt/ctrl_opt_power_control.o" "./common/lib_opt/ctrl_opt_pscan.o" "./common/lib_opt/ctrl_opt_rssi_monitor.o" "./common/lib_opt/ctrl_opt_scanner.o" "./common/lib_opt/host_opt_gap_bond_mgr.o" "../cc27xx_freertos.cmd" -Wl,-lti_utils_build_linker.cmd.genlibs -Wl,-llibc.a [267]../../master/ELFLNK/collect.c:795:internal fatal error #10478: (.TI.bound:dmaChannel5ControlTableEntry) [268]INTERNAL ERROR: C:\ti\ti-cgt-armllvm_4.0.4.LTS\bin\tiarmlnk had an internal inconsistency and aborted [269]This is caused by a defect in the TI Linker. [270]TI Customer Support may be able to suggest a workaround to avoid this. [271]Upgrading to the newest version of the compiler may fix this problem. [272]Contact TI on the E2E support forums at http://e2e.ti.com [273]We need to see this ENTIRE error message and a complete, reproducible [274]test case including ALL of the command-line options. [275]Include all of the object files, libraries, and linker command files [276]used to link the program. [277]tiarmclang: error: tiarmlnk command failed with exit code 2 (use -v to see invocation) [278]gmake[1]: *** [makefile:218: basic_ble_LP_EM_CC2745R10_Q1_freertos_ticlang.out] Error 2 [279]gmake: *** [makefile:212: all] Error 2 [280]**** Build Finished ****