Part Number: TMS570LS1227
Tool/software:
Hello,
I have an application using the Fapi V2.01.01 Build (000830), programming individual bytes with no ECC (to allow contiguous elements of sizes less than 8 bytes) and I am seeing some unexpected behavior when using Bank 7 (EEPROM).
The library is loaded into RAM on startup, and I am storing data in EEPROM. I've noticed that, intermittently, some sort of 'corruption' in the bytes written to EEPROM occurs. I'm writing various elements of sizes between 1-8 bytes in length, but I'll see 1 or 2 bytes within a larger element vary from the intended data. For example, an 8 byte element contained a word whose intended value is 0x4B3E4E61, but the actual value written and seen in the memory browser is 0x4B3E4E41. I can and have actively verified this by reading and comparing the expected to actual data programmed in EEPROM.
I've considered that it could be impacted by the IQR/FIQ, but from what I understand that is only the case if the interrupt were to be performing some other Fapi related call. My IRQ does not make any other Fapi calls.
I believe I am following the recommended programming flow, defined in spnu501h, section 6.3.
I have been unable to identify a failure of the API, per the return values of functions such as Fapi_initializeAPI, Fapi_setActiveFlashBank, Fapi_enableEepromBankSectors, or Fapi_issueProgrammingCommand.
Any help would be much appreciated. I would prefer to avoid re-writing my higher level EEPROM handler to retry when a perceived incorrect write occurs.