Other Parts Discussed in Thread: TMS570LS20216
Hello Forum/Engineers,
I am planning to use TI Hercules MCUs (TMS570LS31xx with included Ethernet and ZWT Housing). I've some concern about the EM Immunity of the Hercules MCUs because the application is suited in the railway sector (high electrical/magnetical fields).
When I read the Safety Manual of the TMS570LS20216S (V 1.0.4) there is mentioned that the product should not exposed to high frequent (> 1MHz) magnetic fields larger than 1.07 A/m . In the actual version of the Safety Manual for the Hercules MCUs there I can't find such restrictions.
Q: What are the restrictions for the TMS570LS31xx regarding the electrical/magnetical field immunity and exists there any detailed description (is 1.07 A/m just for frequency components > 1MHz)?
regards,
logan