Tool/software:
Our MSPM0G1506 design will be battery powered and running nominally at 4MHz when active.
VCC range during the defined lifetime of the battery is 3.0-2.2V
is it feasible to read the VCC rail (channel 7) while the Flash erase/write is active?
Essentially, since the Flash erase/write is my most power consuming event (10mA at 3.3), I want to see how much sag my power rail has during that load. (if possible)
OBTW- what happens to the erase/write current as VCC goes lower?
THANKS for any replies!