Hi,
I have set FMzPLL = 80 MHz = VCLK
The VCLK2R = 0 so peripheral clock should be VCLK/2 = 40 Mhz. But when I measure the SPI data bit SPI2, the bit waveform as below, the bit rate is only 1 Mhz. Why the transfrom is 80:1?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have set FMzPLL = 80 MHz = VCLK
The VCLK2R = 0 so peripheral clock should be VCLK/2 = 40 Mhz. But when I measure the SPI data bit SPI2, the bit waveform as below, the bit rate is only 1 Mhz. Why the transfrom is 80:1?

Hi QJ,
Thanks your advice.
But I did a FMzPLL test yesterday and set the final PLL out to 200MHz, the eval board suddenly lost the link between computer. I tried to reload the program, but failed even if I used the demo software to do. The error message is as below:

How to recover the IC and reset to the original status?
Hi Chang,
1. open norFlash
2. Check "Erase" command, and select "TIXDS100V2" emulator
3. Execute the norFlash
4. While the JTAG is connecting the device, please press "RESET" button on board then release it quickly
5. norFlash should erase the flash correctly.
Regards,
QJ