AM2434: am2434 profinet

Part Number: AM2434

Tool/software:

Hi,TI experts:

        we plan to use the Profinet protocol of AM2434 for the servo drive solution. I have the following questions that I would like to consult:

(1).When is the Profinet solution for AM2434 planned to support the MRPD function?This function is frequently used by customers.

(2).Does TI have a plan to support the PROFIdrive  application layer solution?

     e.g: PROFIdrive Standard telegram:  telegram 1 /telegram 3/telegram 5/telegram 7/telegram 9

           Siemenz telegram : telegram 102 /telegram 105/ telegram 110/telegram 111

(3).PROFINET has introduced PN security levels 1-3 in accordance with IEC62443. Does the protocol stack of AM243x meet these requirements? If not, is there a follow-up plan?

    Siemens has already planned to comply with this standard.Therefore, our product plan must also conform to this standard.

If possible, we would appreciate it if you could provide a specific schedule for the implementation.

 

  

thanks

  • When is the Profinet solution for AM2434 planned to support the MRPD function?This function is frequently used by customers.

    Expected by Nov 2025. 

    .Does TI have a plan to support the PROFIdrive  application layer solution?

    This is part of roadmap. 

    PROFINET has introduced PN security levels 1-3 in accordance with IEC62443. Does the protocol stack of AM243x meet these requirements? If not, is there a follow-up plan?

    Yes, this is part of our roadmap, but we rely on Siemens stack support availability to enable this. HW wise AM243 can meet Class3 requirements based on our assessment.

    Please reach out to your TI sales contact for advanced features support like this.