Other Parts Discussed in Thread: TIDA-010243, , ADS131M08, ADS131M08EVM,
Tool/software:
Hello,
I'm moving up from the MSP430 to the MSPM0 family of MCUs, and I'm looking for help specific to SPI/DMA communication using the MSPM0, similar to what's implemented in TIDA-010243. So, I have 3 questions:
1) What example code, within the MSPM0 development tools, is recommended to use, to test SPI/DMA communications between the MSPM0G3507 [MCU] and the ADS131M08 [ADC], where the MCU fetches data continuously from the ADC?
2) Do the ADS131M08.h/(*.c) files exist, or, would I need to create them?
3) Is it possible to use the MSP Zero Code Studio to develop SPI/DMA communication between the MSPM0G3507 and the ADS131M08? If so, what examples can be recommended?
Thanks for your help.
Best,
Dag.FF2