Part Number: AM2632
Other Parts Discussed in Thread: UNIFLASH
Tool/software:
Hello,
Questions:
Regarding the addresses of the external FLASH shown in the attached diagram:
1. For SBL (0x60000000) and UserSoft (0x60080000), are these addresses physical addresses of the external flash or logical addresses?
If they are logical addresses, could you please provide the corresponding physical addresses?
2. What is the starting physical address of the FLASH that the RBL accesses in order to read the SBL?
3. Is the operation flow described in the attached diagram correct?

Background:
We are trying to program the SBL and the application into Flash using our own tool via JTAG. However, we have not yet been able to make the mechanism work and are currently analyzing the issue.
In addition, if we develop such a custom programming tool, are there any particular points we should be aware of?
Best regards
gokaya