Part Number: TMS570LC4357
Other Parts Discussed in Thread: HALCOGEN
Tool/software:
Is there a way to trigger the FBVECADDR during VIM ECC testing? To confirm that the handler works? This would be the vimECCErrorHandler in the TI HalCoGen.
In the TRM, it is stated that:
The UERR indicates that a double-bit error has been found and that the Interrupt Vector Table is
bypassed. The resulting vector of any IRQ/FRQ interrupt is then the value contained in the
FBVECADDR register until this bit has been cleared.
In 19.9.1 Interrupt Vector Table ECC Status Register (ECCSTAT), but when I triggered a UERR, then attempted to trigger an IRQ/FIQ, I did not see the function at FBVECADDR get called. Is there a formal way to test this at all?
Thanks,
Ben