Part Number: AM2431
Other Parts Discussed in Thread: AMIC110, , AM2432
Tool/software:
Hello, I have a working design in production using the AMIC110 processor, and I would like to update it to run with one of the Sitara microcontrollers. My aim is mainly to reduce power needed to run the board. To do this, I am planning to reduce the I/O voltage to 1.8V for the PHYs and the ADC that I use. This will save a few hundred milliwatts. In addition, I can do without the DDR3 RAM on my board if I use a microcontroller with on-board memory, saving a bit more power.
I have been looking through the formidable array of microcontrollers TI has that support EtherCAT, and I was looking for a recommendation for the lowest power solution. I am using the 83822 PHY, as it seems to be the lowest-power and it works on my AMIC110 based system. The AM2431 seems to be the lowest power microcontroller I've run across that supports the EtherCAT firmware in the PRUs. Do you have any suggestions for me in my quest? I realize it's not exactly a good idea to use EtherCAT in a power-constrained system. It's not up to me!
My secondary aim is to use a supported RTOS, as TI-RTOS is no longer supported on the AMIC110, and FreeRTOS is supported only on newer processors.
Thanks!
John Ford