This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UNIFLASH: Uniflash stopped working while configuring debugger

Part Number: UNIFLASH
Other Parts Discussed in Thread: IWR6843

Tool/software:

Hi there,

I use uniflash to flash precompiled images onto an IWR6843 via an XDD110 Debug Probe.

The process worked well till now - the configuration hasn't changed but now uniflash is stuck while "configuring debugger".

As the confguration worked, I never updated uniflash 8.3 or anything but now it is stuck at "initializing etm_0" before even entering the flashing process.

So I installed the latest version uniflash 9.3 to check if this works out but it stuck at a different file "Parsing C:\ti\uniflash_9.3.0\deskdb\content\TICloudAgent\win\ccs_base\common\targetdb\Modules\radar\DSS_SCI.xml" and keeps working there forever... also before any flashing happens. 

 

So I would suppose this is an software issue as the problem occurs before any flashing of the chip.

Again - the configuration was nevere changed. What did indeed change was the installation of regular windows updates of course but thats all.

 

Any suggestions on where to look or what to try?

Thanks

Steve