This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-MSPM0G3507: DAP Connection Error. This could be caused by the device having gone to low power mode.

Part Number: LP-MSPM0G3507

Tool/software:

[03/10/2025, 13:06:20] [ERROR] CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.
[03/10/2025, 13:06:24] [INFO] CS_DAP_0: GEL Output: Initiating BOOTRST Board Reset
[03/10/2025, 13:06:25] [INFO] CS_DAP_0: GEL Output: Reset line asserted
[03/10/2025, 13:06:25] [INFO] CS_DAP_0: GEL Output: Reset line de-asserted
[03/10/2025, 13:06:25] [INFO] CS_DAP_0: GEL Output: Board Reset Complete
[03/10/2025, 13:06:25] [INFO] CS_DAP_0: GEL Output: Reset done
[03/10/2025, 13:06:26] [ERROR] CS_DAP_0: Error connecting to the target: DAP Connection Error. This could be caused by the device having gone to low power mode. Try forcing an external reset.If the error persists, try forcing BSL, a Mass erase or a Factory Reset. Check device FAQs for more information.

I am pressing switch S2 on lauchpad while force resetting.But these logs are coming again and again. A lot of boards have this issue.I hope this issue gets fixed.
Or please give a solution so that the board doesnt do to this state.