Part Number: MSPM0G3507
Tool/software:
Hello experts,
I am using MSPM0G3507 and would like to double check if my understanding of settings are correct.
(1) ADC
If we want to measure the Temperature Sensor using Internal 2.5V for VREF, is VREF+ connected to Open and VREF- connected to GND, correct?

(2) Pin setting of unused pins
We tried the following three settings for unused terminals, and confirmed that the current consumption is all the same.
Is there any recommended setting out of following 3 for the MCU?
・Input + Pull-up resistor
・Input + Pull-down resistor
・Output Low