This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: SYSOSC clock frequency accuracy

Part Number: MSPM0G3507

Tool/software:

Hello experts,

For the resistor connected to the Rosc terminal,

Could you please tell me clock frequency accuracy under the following conditions?

Parameter Test Conditions MIN MAX
fSYSOSC SYSOSC accuracy when frequency correction loop (FCL) is enabled with ROSC resistor put at ROSC pin, for factory trimmed frequencies(1)

SETUSEFCL=1, -20℃ ≤ Ta 85,

±0.1% ±25ppm ROSC

? ?

SETUSEFCL=1, -20℃ ≤ Ta 85,

±0.5% ±25ppm ROSC

? ?
SYSOSC frequency accuracy when
frequency correction loop (FCL) is
enabled when the internal ROSC resistor
is used (4)
SETUSEFCL=1,  -20 ℃ ≤ Ta 85 ℃               ? ?