This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Flash Programming stops and not finished

Part Number: AM2434
Other Parts Discussed in Thread: LP-AM243

Tool/software:

Hi,

 

We’ve received an inquiry from the customer. Please help to answer their question below.

 

---------------------------------------------------------------

This is a question regarding FLASH writing.

When booting from the sbl_ospi.release.hs_fs.tiimage included in Motor Control SDK v11_00_00_06 after writing it to FLASH, the system stops at the following log output:

---

DMSC Firmware Version 11.0.7--v11.00.07 (Fancy Rat)

DMSC Firmware revision 0xb

DMSC ABI revision 4.0

---

 

On the other hand, when using the same image (sbl_ospi.release.hs_fs.tiimage) from Motor Control SDK v09_02_00_12, the system continues beyond the above log and boots as expected.

Has the image included in SDK v11_00_00_06 been verified to work correctly?

If so, could you please advise on possible causes for the system stopping at this stage when using the v11 version?

---------------------------------------------------------------

 

Thanks and regards,

Hideaki