This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LC4357-EP: Special external oscillator?

Part Number: TMS570LC4357-EP
Other Parts Discussed in Thread: TMDX570LC43HDK

Tool/software:

Hi Experts,

Would like to ask about TMS570LC4357-EP:
What is the recommended frequency for an external oscillator used with this enhanced product MCU in the subject line? Is there a preferred oscillator that is recommended by TI to use in junction with this MCU?

From dev't kit TMDX570LC43HDK with catalog variant of MCU, using 7A-16.000MAAJ-T external oscillator but in narrow opTemp. Wondering if the external oscillator below shown from mouser can be used?

Thank you.

Regards,
Archie A.

  • Hi Archie,

    ECS-160-20-30B-DU Specifications vs Requirements:

    1. Frequency: 16.000 MHz
    • This matches exactly with the development kit's oscillator frequency.
    • Falls well within the acceptable frequency range (5 to 20Mhz) for the TMS570LC4357-EP
    1. Temperature Range:
    • ECS-160-20-30B-DU operates from -55°C to +125°C
    • This is also matching with controller operating temperature range.
    1. Stability: ±30 ppm
    • This stability is generally acceptable for automotive applications
    • The oscillator monitor on the TMS570LC4357-EP will help ensure proper operation
    1. Load Capacitance: 20pF
    • Falls within the typical 12-24pF range for TI MCUs
    • Compatible with the TMS570LC4357-EP requirements

    I didn't see any issues in using this crystal for TMS570LC4357-EP controller.

    --
    Thanks & regards,
    Jagadish.