Part Number: TM4C123GH6PZ
Tool/software:
Hi all,
As the title, error-1170 occurred while debugging.
The following information showed the environment of the work.
If more information are needed, please let me know.
-IDE: CCS Version: 9.2.0.00013
-Debug tool: XDS200
-Description:
Previously, we changed the ARM MCU from MSP432 to TM4C.
After the troubles which were occurred with the development with the launchpad were solved, we designed a new PCB.
The PCB has almost the same functions as the one with MCU, MSP432P401R.
As soon as the sample PCBs were finished, I made several PCBs and check the debugging and/or download firmware to TM4C123GH6PZ.
All of the them can be debugged completely but one of them met the error-1170 when it did the same operation again.
I have met the some trouble while using launchpad.
It is solved by using LM Flash Programmer to erase the firmware of the launchpad but not this time.
I have tried to reset the power of the PCB, reset the XDS200, and have tried all I could do.
(Note: other PCBs can be debugged with the same PC, same XDS200 and other settings.
The project for debug operation is an empty project, I do not the the operations of the code would cause the trouble.)
I think the trouble was the settings of the MCU or the bad status of the chip.
How can I solve the trouble?