Part Number: MCU-PLUS-SDK-AM263X
Tool/software:
Hi,
I have a AM263X launchpad, and i need to create a "safe_image", responsible to execute updates firmware commands from external application. Basically, the safe_image should be called after the SBL, like a application image, but the safe_image happens before the application image. The safe_image need run a application image, located on flash, like a SBL.
I tried create the safe_image based on sbl_qspi, from TI SDK, with the bootloader offset to run the application image on correct flash position, but i cannot run this correctly.
In my case, the SBL its load on 0X60000000, and the safe_image (based on SBL), its loaded on 0X60080000. The application image its load on 0x600C0000, and in the safe_image syscfg, the offset its 0X000C0000, so, the expected behavior its the sbl start and run the safe_image, and the safe_image runs the application_image.
This is correct? Whats the best choice to create this safe_image? Basically, i need to jump from the safe_image to application_image.
Other question is, i need create the safe_image as tiimage or appimage?
Bests regards,
Gabriel