Part Number: RM57L843
Other Parts Discussed in Thread: ADS7953
Hi,
Here is what I am trying to do, but I am having some difficulties finding all the information.
I want to trigger SPI transfers using a timer. I was thinking of using one of the N2HET timers to trigger the SPI transfer.
I plan on using the SPI in DMA mode, and trigger SPI transfers periodically.
I am assuming that if I configured the corresponding CS pin in functional mode (PC0 register), the CS signal would handled automatically by the SPI peripheral.
Is this even possible?
To understand why I want this, I need to use the ADS7953 for ADC conversions and read back the converted values of multiple channels using the setup. It is configured in manual (single shot) mode, so I need to issue a separate SPI tranfser for each channel that I want to read.
I am assuming that if I configured the corresponding CS pin in functional mode (PC0 register), the CS signal would handled automatically by the SPI peripheral.
Thank you for your help
Michal Solecki