This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4-Q1: ADC input protection

Part Number: AM263P4-Q1

Dear Experts,

I have a question regarding the ADC pins of the AM263P4-Q1 and its protection.

The Technical Reference Manual states, that each ADC pin has a CMPSS connected in parallel:

2025-10-16 17_35_11-AM263Px Sitara Microcontrollers Technical Reference Manual (Rev. B) - AM263P_tec.png

 

The Specification of the CMPSS states a Failsafe Input Current Injection of 10mA:

2025-10-16 17_37_02-_ AM263Px Sitara™ Microcontrollers with Optional Flash-in-Package datasheet (Rev.png

Does this mean that each ADC pin can whithstand up to 10mA when loaded whith voltages higher than VDDA or are we misinterpreting the data?

Thanks!