Part Number: MSPM0G1106
Other Parts Discussed in Thread: SYSCONFIG,
Description: Two developers built the same CCS project from the same Git respository with the latest changes. However, the resulting .bin files differ.
Environment:
IDE: Code Composer Studio (Version: 12.7.1.00001)
SDK: MSPM0 SDK (Version: 2.1.0.03)
Compiler: TI Clang v4.0.0.LTS
SysConfig: 1.19.0
Target device: MSPM0G1106
Steps to Reproduce:
Both developers pulled the latest changes from the same repository (git log confirms same commits).
Project cleaned and rebuilt on both machines.
Resulting .bin files compared using cmp; differences found.
File names made identical; result still differs.