This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1106: mspm0c1106 supported version

Part Number: MSPM0C1106

Hello, 

I have LP-mspm0c1106 board and I want ask, If this msp is supported in CCS version 12.8.1. 

Thank you

  • Hi Jan,

    The MSPM0C1106 is supported in CCS v12. I would highly suggest installing the latest SDK. In order to ensure you can import and develop projects for the device, you need to have the latest Device Support Package for MSPM0.

    The latest version is 1.16

    You can find what version you have using the following steps:

    1. Help > About Code Composer Studio
    2. Click on Installation Details in the bottom left corner of the window that pops up
    3. Scroll down and see if you can find this (ignore the version in the screenshot):
    4. If you don't find this, follow the steps below

    How to download the latest Device Support Package for MSPM0:

    1. Uninstall CCS v12 and reinstall
    2. During the reinstall, make sure you select the option for Device Support Package for MSPM0

    Best,

    Owen

  • Thank you very much for answer. 

    I looked to ccs and find this

    Is that it ? If no, It is possible install mspm0 without uinstall ccs ?

    Iˇm asking because I can't create a project for MSPM0C1106 in project wizard.

    Thank

  • Hi Jan,

    I will get in contact with our software team and get back to you as soon as possible.

    Best,

    Owen

  • Hi Jan,

    Sorry for the delay. After working with the software team, they seem to have resolved this issue. Try these steps:

    1. Help > Check for Updates
    2. You should then see this:
    3. Click Next
    4. Click Next again
    5. Agree to the terms and click Finish
    6. You'll then be prompted to restart Code Composer Studio
    7. Up restarting, you should now be able to create projects for the MSPM0C1106 using the project wizard

    Best,

    Owen

  • Thank you very much,

    It helped me and I can now create the program.

    But I would like to ask, I think there wasnt this update option before. Did you add it there ?

    Best,

    Jan

  • Hi Jan,

    Glad to hear that this resolved this for you too.

    The software team added this upon bringing the issue to them. Thanks for sharing this with us.

    Best,

    Owen