This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0C1104: CCS to Factory reset the C1104

Part Number: MSPM0C1104

Champs:

By using the CCS script, I can erase the M0 to the C1104.

But using the Facory reset "Auto" to the C1104, it will bring me the below error.

how to fix?

BR Rio

 

S_DAP_0: GEL Output: SEC_AP Reconnect
SEC_AP: Error connecting to the target: (Error -615 @ 0x0) The target failed to see a correctly formatted SWD header. The  connection to the target may be unreliable. Try lowering the  TCLK setting before trying again. (Emulation package 9.13.0.00201) 
CS_DAP_0: GEL: Error while executing GEL_DAPInit_SECAPCommand(): Connect failed
     at GEL_Connect()
     at GEL_EvalOnTarget("SEC_AP", "GEL_Connect()", 1) [mspm0_cs_dap_init.gel:385]
     at GEL_DAPInit_SECAPCommand()