Part Number: EK-TM4C1294XL
Other Parts Discussed in Thread: TM4C1294NCPDT,
Setup Details
Device: TM4C1294NCPDT (EK-TM4C1294XL board)
TivaWare Version: 2.2.0.295
Compiler: TI Arm Clang 4.0.3.LTS
Project: enet_tcpecho_server (from examples/boards/ek-tm4c1294xl/)
Path Root: E:/TIX (TivaWare extracted here)
lwIP Folder: E:/TIX/third_party/lwip-1.4.1/
Current Problem
The compiler throws:
E:/TIX/third_party/lwip-1.4.1/src/include/lwip/tcp.h", line 41: fatal error #1965: cannot open source file "lwip/ip.h"
On inspection, I noticed that in my TivaWare installation, the folder
E:/TIX/third_party/lwip-1.4.1/src/include/lwip/ does not contain ip.h.
The only ip.h present is under:
E:/TIX/third_party/lwip-1.4.1/src/include/ipv6/lwip/ip.h
There is no ipv4/lwip folder, and no top-level lwip/ip.h either.
What I Suspect
Either the IPv4 headers are missing from this TivaWare installation (possibly incomplete extract),
Or this version of enet_tcpecho_server depends on a different lwIP 1.4.1 variant that included IPv4 headers.
Help Requested
Could you please confirm:
Whether the lwip/ip.h file (and ipv4/lwip/ip.h) should normally exist in TivaWare_C_Series-2.2.0.295?
If yes — can you share the correct lwIP 1.4.1 folder structure (or link to the proper version)?
If the example was updated for IPv6-only, is there a documented way to adapt the enet_tcpecho_server project to the available lwIP tree?
Is there any official patch or updated lwIP package recommended for TM4C1294 Ethernet examples?