Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2434: Hardware integrity up to SIL Standard

Part Number: AM2434

Hi,

Our project requires a processor/controller that supports IEC 61508 hardware integrity up to SIL 3 with the following memory specifications:

  • 512 MB SDRAM

  • 256 MB NOR Flash

  • 1 GB NAND Flash

The AM2434 meets the memory requirements but does not support SIL3 hardware integrity.
The AM263x supports SIL3 hardware integrity, but its RAM capacity is less than 512 MB.

Please help us identify a suitable processor/controller that meets both the SIL3 safety and memory requirements, or suggest any alternative solution or approach to achieve this.

Thanks,

Regards,

Veerappan P.