This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] AM2612: Zephyr

Part Number: AM2612

 Loudspeaker Announcement: Zephyr RTOS Pre-release available on the AM261x SoC!

We’re excited to announce that preliminary support for Zephyr RTOS is now available on the AM261x microcontroller. This integration unlocks a modern, highly scalable, open-source operating system for developers building industrial networking and real-time applications on the AM261x platform.

---

 Dart Why Zephyr on AM261x?

Benefit What it means for you
Low‑Latency Real‑Time Performance Deterministic scheduling and submillisecond interrupt latency for time‑critical workloads
Modular Architecture Pull in only the kernel features you need, keeping binary size minimal (as low as a few KB)
Device‑Tree‑Driven Configuration Simplifies board bring‑up and peripheral enablement with a single source of truth
Extensive Community & Vendor Ecosystem Leverage a growing library of drivers, middleware, and sample applications

 Rocket Getting Started

1. Toolchain Setup


- Install the Zephyr SDK (v0.16.1 or newer).
- Use the recommended GCC‑Arm Embedded toolchain (`arm-none-eabi-gcc >= 10.3`).

2. Clone the Zephyr fork from TI Github

west init -m https://github.com/TexasInstruments/zephyr/tree/am261x/release zephyrproject
cd zephyrproject
west update


3. Select the AM261x LP

Zephyr now ships a ready‑to‑use board definition: `am261x_lp`


west build -b am261x_lp samples/hello_world

4. Flash the Image

Use existing tools like TI Uniflash GUI tool to flash the image. Steps here
More info - Link

5. Debugging


It is recommended to use CCS for flashing & debugging the binary image. Steps here 

More info - Link

6. The key enablement in the first release

Launch Pad support for AM261x
R5F (arch) support for interrupts, Cache, MPU configs
IOMUX controls via pinctrl
Systick support with RTI as Tickless Kernel enablement
MBox Driver enabled in compatibility with IPC notify Layer
UART, GPIO Peripheral Support

 Books Resources

Resource Links
Zephyr RTOS Documentation https://docs.zephyrproject.org
AM261x Hardware Reference github.com/.../index.rst
Getting Started Guide (PDF) www.example.com/.../zephyr‑quick‑start.pdf 
Community Forum forum.zephyrproject.org/.../am261x
Sample Repository github.com/.../am261x

 Handshake Support & Feedback

- Technical Support: Open a ticket in the E2E forum (Tags “Zephyr – AM261x”).
- Community Contributions: Pull requests adding drivers, board configurations, or sample applications are always welcome!

---

 Tada Let’s Build the Future Together!

The AM261x series now has the power and flexibility of Zephyr RTOS at its fingertips. Whether you’re prototyping a Motor Controller or a small robot, Zephyr gives you a modern, open‑source foundation to accelerate development.

Happy coding!

The AM261x & Zephyr Integration Team