Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G1519: Changing CLK2X_DIV on the Fly

Part Number: MSPM0G1519

Hello.

I am generating GPIO data patterns via DMA and a LUT; all works good.

I want to change how long the LUT takes to be output to the GPIO to reduce LUT size (not use padding).

I have been changing CLK2X_DIV on the fly and it seems to work; this may not be "safe"....do I need to disable the PLL ? 

Since the divider is at the output of the PLL (and not in a feedback loop) then one would hope the CLK2X_DIV update is synchronised accordingly to avoid any runt pulses....????

Can't find anything in the TRM about it.

Code is:

gSYSPLLConfig.rDivClk2x=0x0f; //div 16 (20 MHz)
DL_SYSCTL_configSYSPLL( &gSYSPLLConfig);
 
DO DMA
 
gSYSPLLConfig.rDivClk2x=0x03; // div 4 (80 MHz)
DL_SYSCTL_configSYSPLL( &gSYSPLLConfig);
 
--
Thanks
 

 

 

 

  • Hi Philip,

    Is there anything else in your system that is going to be impacted by this change in the MCLK frequency? Timers, communication peripherals etc.

    The driverlib function DL_SYSCTL_configSYSPLL( &gSYSPLLConfig); will disable the syspll, adjust all settings, then reenable the syspll and wait. If your pseudo code accurate, I don't foresee any issues.