Part Number: MSPM0L1306
Other Parts Discussed in Thread: UNIFLASH, ,
Hi there,
When I try to flash the secondary_bsl_uart example from CCS, flashing fails.
However, when I use UniFlash to load the same .out file, it flashes successfully. Is there any additional step or setting that I am missing to flash the secondary_bsl_uart example correctly on LP-MSPM0L1306?
Environment:
-
Hardware: LP-MSPM0L1306 LaunchPad (on-board XDS110)
-
SDK: mspm0_sdk_2_06_00_05
Example used:C:\ti\mspm0_sdk_2_06_00_05\examples\nortos\LP_MSPM0L1306\bsl\secondary_bsl_uart
Steps to reproduce:
-
Import the
secondary_bsl_uartexample into CCS. -
Build the project successfully.
-
Open Debug Configurations → erase configuration: erase MAIN und NOMAIN memory.

-
flash from CCS.


here is my hardware setup: