Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
Hi champs,
I am asking this for our customer.
The user wants to have up to 3x open-drain output pins with external pull-up resistors in order to save power consumption on MSPM0.
1) The user can use PA0 and PA1, where no internal pull-up resistors are connected. Is it right?
2) But they still need the 3rd pin. Can standard drive IO pins be used as open-drain output pins by software congurations?
(3.3V is needed. No need for 5V.)