Part Number: AM263P2
Hello~~
Question about AM243P2 temperature sensors
1. How many temperature sensors are there inside?
The TRM document shows four.
TSENSE_CFG_SENSOR_SEL
bit3:temp_sensor3
bit2:temp_sensor2
bit1:temp_sensor1
bit0:temp_sensor0
2. Please explain the purpose and location of each sensor.
3. When connecting an additional temperature sensor to check other devices outside the CPU, is it possible to use the ADC pins for interrupt operation?
4. If only a specific ADC pin needs to be used as an interrupt, please provide the pin number.
Thank you
Jongho Park