Part Number: MSPM0G3507
Hello, for an automotive project, I'm trying to create a stable memory mapping for the MAIN region of the flash, that includes the following:
- 8kB flash area used as NvM (no emulation).
- interrupt vector mapped at adress 0x0000 2000, and using the VTOR register to specify this.
- rest of the memory reserved to the application.
I've attached a diagram showing the above mentioned areas. Can you please let me know if there are any issues with the proposal? Thanks!