This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM2432: Please Provide IBIS AMI models

Part Number: AM2432

Hi,

My customer needs the AMI simulation model for PCIe simulation.

Could you provide it to them ?

They tried sprm730e.ibs model, but the following pins were NC.

Y15        SERDES0_RX0_N            NC
Y16        SERDES0_RX0_P            NC
AA16     SERDES0_TX0_N            NC
AA17     SERDES0_TX0_P             NC

Also, they found the following comment at the line 56 to 58 in the sprm730e.ibs model.

Could you please provide the IBIS AMI models.

----------------------------------------------------------------------

  This file does not include AMI models for SerDes based links.

  For SerDes simulations use Texas Instruments IBIS AMI models

  Some IV curves contain Non monotonic data points.

----------------------------------------------------------------------

 

Thanks and regards,

Hideaki