Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1117: UART Fractional Baud Rate Clock Generation

Part Number: MSPM0L1117

Hello,

How is the fractional baud rate clock generated? In the MSP430 TRMs they describe using a modulator to generate a fractional clock but the MSPM0 doesn't describe if that's what's happening here.

Or does the UART peripheral just insert 1 UARTCLK every once in a while to get an "average" correct frequency?

Munan

  • There are difference between MSP430 and MSPM0 baud rate generation.

    Here is the feedback from 3rd:

    The bit rate generator on the MSP430 is quite different. The modulation pattern is fixed and restarts with each start bit.

    For the MSPM0: please refer to TRM: UART section 23.2.3.4 Baud Rate Generation

  • Hi Helic,

    Highlight for me where in here it actually describes how the fractional baud rate generation WORKS. 

    All I see is that you can set a fractional baud rate divisor from 1 to 64. That doesn't describe how this gets generated or what the timing diagram might look like for the fractional bits.

    Munan

  • Hi,  

    TRM didn't provide these detailed information.'

    Is this a customer required information?

    If yes, please try to contact me offline and provide detailed information.