Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
I tried to set a breakpoint inside the break-error interrupt, but it never triggered. The receive function is working, but I’m getting an error in PLIN VIEW PRO saying “slave not responding,” which means the TX is not working.
Additionally, I am using the ATA663211 transceiver, and the connections are made with the MSPM0G3507 controller like below. Is this correct? Because in the linked project (www.ti.com/.../slaaek9.pdf, the connections are crossed — TX to RX and RX to TX.
TX (ATA663211) → TX (PA0 – MSPM0G3507)
RX (ATA663211) → RX (PA1 – MSPM0G3507)
I have also attached my configuration(syscfg) file's screenshots.
Currently, I have connected: