Part Number: AM263P4
Other Parts Discussed in Thread: TMS570LC4357
Hi, I'm exploring which MCU to use for our next project.
Currently I'm looking at AM263P4 and have question about usage of OSPI. We were planning to connect PSRAM and flash to OSPI using different chip select. But studying it revealed that it might not be possible to do like this?
When I was using EMIF of TMS570LC4357, I was able to connect SDRAM as synchronous device and vfpga as async2. Accessing different address spaces starting from 0x6000 0000 and 0x8000 0000 automatically handled chip selects.
I read AM263P4 memory map and it seems OSPI address space is not separated by chip select and all 3 segments direct access to same physical device, chip select chosen by register. So unless I manually switch which device to access, I can't use both device to use. Is this correct?