Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0L1228: Issue with Implementing Inter-Byte Delay in I²C Master Mode on MSPM0L1228

Part Number: MSPM0L1228

As per the MCF8316C driver requirement, the master IC must introduce an inter-byte delay of 100 µs between each byte for reliable communication during both transmission and reception.

I have implemented the logic and successfully observed the delay between bytes in most cases. However, there is one limitation:

  • I am unable to introduce the inter-byte delay between the START condition and the first data byte during reception.
  • For all other bytes, the delay works as expected.

Question:
Could you please guide me on how to achieve this requirement in master mode? Specifically:

  • Is there any way to insert a delay between the START condition and the first received byte?
  • Are there any recommended approaches or hardware features in MSPM0L series that can help implement this?

Additional Details:

  • MCU: MSPM0L1228
  • Communication: I²C Master Mode
  • Requirement: 100 µs inter-byte delay for MCF8316C driver compliance