Part Number: MSPM0G3519
Hi,
I am trying to flash the MSPM0G3519 using jlink, but I am running into the following issue.
SEGGER J-Link Commander V8.84 (Compiled Nov 5 2025 18:42:50)
DLL version V8.84, compiled Nov 5 2025 18:41:46
Connecting to J-Link via USB...O.K.
Firmware: J-Link V12 compiled Oct 15 2025 16:56:26
Hardware version: V12.00
J-Link uptime (since boot): 0d 02h 05m 35s
S/N: 52011251
License(s): GDB
USB speed mode: High speed (480 MBit/s)
VTref=3.295V
Type "connect" to establish a target connection, '?' for help
J-Link>con
Please specify device / core. <Default>: MSPM0G3519
Type '?' for selection dialog
Device>
Please specify target interface:
J) JTAG (Default)
S) SWD
T) cJTAG
TIF>S
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "MSPM0G3519" selected.
Connecting to target via SWD
InitTarget() start
DAP initialized successfully.
No PWR-AP detected.
InitTarget() end - Took 402ms
Found SW-DP with ID 0x6BA02477
Failed to power up DAP
InitTarget() start
DAP initialized successfully.
No PWR-AP detected.
InitTarget() end - Took 299ms
Found SW-DP with ID 0x6BA02477
Failed to power up DAP
Error occurred: Could not connect to the target device.
For troubleshooting steps visit: https://kb.segger.com/J-Link_Troubleshooting
J-Link>