Part Number: AM2634
I'm using teh example dcc_am263x-cc_r5fss0-0_nortos_ti-arm-clang to test lockstep using SDK version am263x_10_02_00_13
when I run the example on lunchpad I got the following result (I didn't edit the example)
[Cortex_R5_0] R5 CPU Application
CCM Example Test Started: R5F0
MCU ESM Initialization completed
CCM Test Init completed
CCM Verify Init completed
CCM Functional Test
CCM self test: starting
CCM self test failed
CCM SelfTest: failure on line no. 337
CCM Functional Test failed for CCM_R5F0
CPU Functionality
Failed.
Some tests have failed.