Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSPM0G3507: DMA features in MSPM0G350x

Part Number: MSPM0G3507

Hello!

Is there anywhere explicit information about which DMA variant is used in MSPM0G3507, DMA_A or _B?

Because I see Repeated Mode and Channel Cascading works on my board, but Gather Mode seems like not implemented in driverlib (disabled by preprocessor as not supported).

I tried to configure it with bare registers, but I'm not sure - if I do something wrong or it is not supported at all? TRM and Driverlib has contradictions here. Or it is just not implemented in driverlib.

Questions

  1. Which DMA variant is implemented in MSPM0G350x, DMA_A or DMA_B?
  2. Does Gather Mode supported by MSPM0G350x?

From MSPM0 G-Series 80MHz Microcontrollers, SLAU846C – JUNE 2023 – REVISED AUGUST 2025:

image.png