Part Number: TMS570LS2124
Other Parts Discussed in Thread: HALCOGEN
Hello . I have several question about MIB-SPI and Compatibility mode SPI .
Can I use the same SPI module for example SPI1 or SP5 both modes (MIB-SPI and compatibilty) to get access to the defferent devices with different chip selects signal. for example - the compatibilty mode used to get information from One SPI Slave and after receiving information, we switch to the MIB mode to receive information from another slave with different chip select. After receiving information from second one, we swith off MIB and consequently get information from first device in compatibility mode - etc...
I ask about this one because I get problem with device which communicated in compatibility mode, after switching on MIB-SPI.
And next question - I can switch on MIB-SPI mode only once after reset, All next writing to the register MIBSPIE were ignored as 1 as 0. Is it normal behaviour? May be I need permit the reinitialization MIB RAM after RESET Initialization?
Best regards
Andrii Shevchuk
Best regards.
Andrii Shevchuk