Part Number: AM2612-Q1
Other Parts Discussed in Thread: SYSCONFIG
Hi experts,
Good day! I am asking for customer.
My customer is developing AM261-Q1.
- They checked the SBL code logic, it first load and run on core 1, then core 0.
The customer wants to know if it is possible to run core0 loads first and then core 1 loads and runs.
2. My customer is facing flash_open issue on their board with their application code.
a. When OSPI and port is configured with Sysconfig, then when they debug ospi_flash_io_am261 demo, they can operate flash successfully. ButWhen OSPI and port is configured with MCAL, they it fails on flash operation.
b. When OSPI and port is configured with sysconfig, then it successes on flash operation. In this successful sysconfig configuration OSPI input frequency is 166MHz.
If they change OSPI input frequency to 133MHz in sysconfig, then it will occur same issue.
But they are using ZSZ package, in theory, 133 Mhz was reasonable, but now it has failed.
c. When OSPI(except port) is configured with sysconfig, port is configured with mcal, then it also fails.
Customer has tried skip_hw_init in their application code, but the issue is not solved. flash can't be operated, other peripherals are normal.
Could you help to check ASAP?
Thanks!
Best Regards
Kita