Part Number: MSPM0C1103
Hi,Experts
I was considering outputting PWM at 5V open drain,
but because an H output occurs during HiZi mode during reset,
I am also considering PWM output at 3.3V.
I checked the datasheet, and it seems that with the MSPM0C1103,
if you allocate one voltage capture ADC, you cannot allocate two 3.3V outputs
unless you use the debug port. Is this correct?
If there is a way to output 3.3V PWM while using the debug port for debugging, please let me know.
It seems like I should be able to use it at 3.3V if I pull up the two open drain systems to PA24 (pin 8),
setting PA24 to L when powered on and H when operation begins.
Is it possible to use it like this?
Best Regards,
Hidekazu