Part Number: AM2612
Other Parts Discussed in Thread: UNIFLASH, TCA6408
Hi,
My customer has a problem on Flash programming using Uniflash (JTAG session). We need your help.
They’re using QSPI Flash (IS25LP128) which meets the requirement described in AM261x OSPI, QSPI Flash Selection Guide.
And, they’re following the procedure in Adding Support For a Custom Flash Device.
They set “flasher_jtag_uniflash.out” In the [Custom Flasher] of [Settings & Utilities] in UniFlash due to using Custom Flash.

In order to create “flasher_jtag_uniflash.out”, they referred to the following project.
C:\ti\motor_control_sdk_am261x_10_02_00_07\mcu_plus_sdk\tools\flasher\jtag_uniflash\am261x-lp\r5fss0-0_nortos
However, this project is created for the architecture using TCA6408 on LaunchPad, but it is not used on their board. Therefore, the error occurred at the setting TCA6408 in the initialization.
Could you help to give them any advice to solve this problem on their board which doesn’t have TCA6408 ?
Is there any example which is not using TCA6408 ?
Thanks and regards,
Hideaki