Part Number: MSPM0G3507
Other Parts Discussed in Thread: SYSCONFIG
Hi All,
Confirmation regarding the SysPLL errata:
Does this issue occur on all G-series devices, but the probability of occurrence is random?
I have a question about the following statement in the SysPLL errata:
>>The count will vary depending on the combined clock accuracies, so it is recommended to add a >>+-5% to allowed range.Estimated time for FCC is 30us.
Does this mean that SysPLL originally has a ±5% error?
Or is it because of this issue that the error has become ±5%?
For example, does the ±1% error of SYSOSC described in the datasheet need to be considered as ±5% after passing through SysPLL? Was this already determined before the errata was issued?
If the FCC value is incorrect, disable and reenable the SYSPLL by setting SYSPLLEN to 0 then 1. Rerun the FCC check.
Regarding this, should I loop the process of setting SYSPLLEN from 0 to 1 and rerunning the FCC check until SysPLL is locked?
Best Regards,
Ito