This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM263P4: Doubt regarding EPWM base addreses

Part Number: AM263P4

I am attaching two screenshots and my doubt is why is the base address for EPWM01_G0 is different in both the screenshots and also what is the meaning of G0, G1, G2 and G3Screenshot 2025-12-01 151425.pngScreenshot 2025-12-01 151308.png

  • Hi,

    https://dev.ti.com/tirex/explore/content/am26x_academy_10_02_00_03/_build_am26x_academy_10_02_00_03/_images/AM263x_SoC_Interconnect.png

    As you can see in the image, to allow access from multiple R5F cores and to avoid latencies due to bus arbiration there are multiple ports to access the epwm regsiters for different cores.

    Please refer to TRM section: 3.9

    PWM interconnect are divided into 4 groups G0_EPWM, G1_EPWM, G2_EPWM and G3_EPWM accessed using different address regions in the memory map. Any initiator can access an EPWM group while another initiator is accessing a different EPWM group simultaneously. Each interconnect System Interconnect Incorporated has n target ports depending on number of EPWM in the design. After the interconnect, a 4:1 Static Mux can be configured per EPWM using CONTROLSS_GLOBAL_CTRL.EPWM_STATICXBAR_SEL0 & CONTROLSS_GLOBAL_CTRL.EPWM_STATICXBAR_SEL1 register, which statically assigns that EPWM to any of the selection groups – G0 to G3.