Part Number: AM263P4
Other Parts Discussed in Thread: TMDSCNCD263P
Hello, I'm currently using the am263px control card (TMDSCNCD263P) to establish CAN communication between two boards.
The first board is supposed to transmit messages, and the second board is supposed to receive messages and send ACK/status replies. However, I'm currently experiencing an issue where the transmission itself isn't working. When I check with an oscilloscope, I see no waveform at all.
I'm currently using the "mcu_plus_sdk_am263px_11_00_00_19" SDK.
Is the failure of CAN communication due to LD8 on the board, "PMIC Safety Error Output (LD8)?"Currently, the LD8 LED on my board is on, and I understand that the default state is off.
The code below is the transmitting part.
thank you.